AXIS#.MOTOR.TEMPSOURCE

Description

This parameter selects the connector used for the motor temperature measurement when the axis motor control algorithm does not use a position feedback (when AXIS#.MOTOR.TYPE = 2 or 10). The temperature sensorClosed A sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer is a thermal resistor connected to the drive through a 2-wire input. The type of thermal resistor is set with AXIS#.MOTOR.RTYPE.

The range of available AXIS#.MOTOR.TEMPSOURCE values are determined by the set of drive connectors. The connectors that support temperature measurements are full 15-wire connectors (X23) and Smart Feedback Adapter (SFA) devices (X1 and X2 with SFA).

When AXIS#.MOTOR.TYPE is not 2 or 10, AXIS#.MOTOR.TEMPSOURCE is not used.

Versions

Action Version Notes
Implemented 02-06-01-000

General Information

Type

Read/Write

Units

N/A

Range

Depends on drive model

Default Value

1

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.